Does Endura support bi-directional audio transmission?

Issue

How to achieve bi-directional audio with Endura.

Product Line

Pelco Video Management, Pelco Transmission & Power

Environment

Endura WS5000/WS5200

Cause

Application to "talk back" to Camera Locations is required.

Resolution

At present, Endura Viewing Stations (WS5200/VCD5200) can receive audio from Cameras/Encoders, but have no support for transmission of audio back to Camera Locations.

To achieve transmission of audio back to the Camera locations, a third-party audio solution must be utilized; One such example configuration is outlined below.

Example third-party equipment
1x Louroe Verifiact L-DT Microphone (LE-079), or other industry-standard microphone device.
1x Louroe DA-8 Audio Distribution Amplifier (LE-275), or other Audio Distribution Amplifier.
1x-8x Louroe or other Remote Speaker(s).

Installation
Refer to the below diagram. For more details, see the Louroe DA-8 Installation/Operation Manual.

 

 

 

West Penn 452 2 Conductor shielded, 22 gauge with a 24 gauge drain wire