What is required for the DX8100 DVR to control a Pan & Tilt motor such as the PT1260EX?

Issue

What receiver driver can be used with the PT1260EX and DX8100 DVR?

Product Line

Pelco Cameras

Environment

  • ERD97P21-U
  • PT1260EX
  • DX8100

Cause

 Integrate the explosion proof PT1260EX to be controlled from the DX8100 DVR.

Resolution

Integration of the DX8100 to control the PT1260EX requires a 3rd component such as a Receiver Driver.The ERD97P21-U which is a receiver driver serves as the conversion device for receiving the Pelco protocol communication (as data input), and then changing it to voltage output to drive the Pan/Tilt device (PT1260EX) 

The ERD97P21-U will accept input of data in the following format:

  • Protocol: Pelco P
  • Baud Rate (selectable): 2400, 4800,9600


The ERD97P21-U will output either of the following voltages through Terminal Block Selection:

  • 24 VAC Pan/Tilt power output (block selected)
  • 120/230 VAC Pan/Tilt power output (block selected)

 

View the related articles below for additional information: