Internet Explore stopped this site from installing an ActiveX control on your computer.

Issue

ActiveX is required to view an IP Camera.

Product Line

Pelco Cameras, Pelco Video Management

Environment

Internet Explorer most recent versions

Cause

Internet Explorer security settings are preventing the software install.

Resolution

Possible Message:

Internet Explorer stopped this site from installing an ActiveX control on your computer. 

1. Select the Internet TOOLS tab from a open browser page.

2. Select Internet Options.

3. Select the SECURITY tab.

4. Select CUSTOM LEVEL.

5. Now scroll down and find ActiveX controls and plug-ins.

    a. Find allow previously unused ActiveX controls to run without prompt, change to Enable.

    b. Apply and Save changes, now exit.

6. Close and re-open your Internet Explorer browser.

CAUTION: Make sure when finished to change the setting back to disabled.