Does the Pelco Mobile application support virtual PTZ (Pan Tilt Zoom) of the Oncam Grandeye Evolution 360 degree IP camera

Issue

Virtual PTZ (Pan Tilt Zoom) functionality of the Oncam Grandeye Evolution 360 degree IP camera 

Product Line

Pelco Cameras, Pelco Video Management

Environment

  • Oncam Grandeye Evolution 360
  • DigitalSENTRY Series

Cause

Dewarping of the Oncam Grandeye Evolution 360 degree IP camera not supported by Pelco Mobile Application  

Resolution

Virtual PTZ (Pan Tilt Zoom) functionality of the Oncam Grandeye Evolution 360 degree IP camera is not supported by the Pelco Mobile application; however, Virtual PTZ (Pan Tilt Zoom) of the Oncam Grandeye Evolution 360 degree IP camera is supported by the Oncam OnVu360 mobile application. Available via the Oncam website at  http://www.oncamgrandeye.com/security-systems/security-software-app/.

 

Just in case it is needed, and to find the OnCam cameras on a Network, try using their Configuration Utility located within that link.