What is the part number for the BNC wiring assembly that exits base of Esprit?

Issue

 What is the part number for the BNC wiring assembly on the Esprit?

Product Line

Pelco Cameras

Environment

  • ES4036 Series
  • ES41P36 Series

Cause

BNC cable replacement due to damage.

Resolution

The Esprit series feature an exiting coaxial cable out of the base transformer. The coaxial cable is RG174/U type with RG174 bnc. The cable is factory length at 36" inches.It is primarily recommended to send in the base transformer for repair should the cable require service. The option of purchasing a cable is possible. Should a repair option be considered, refer to the base transformer label for model number.

Part# WA04-0003-006B. This part can be ordered through a Pelco dealer. Part numbers are subject to change without notice.