PMCL524FL Will select the HDMI input as the primary source upon power up.

Issue

The option to select another source input is restricted to the HDMI as the primary Input.

Product Line

Pelco Monitors

Environment

  • PMCL524FL

Cause

  • Site application requires the VGA to remain as the primary input source during a power outage.

Resolution

The PMCL524FL features support for the HDMI input to be the primary input upon power up.