What is focal length of the Spectra HD S5220 and S5230 IP PTZ cameras?

Issue

What is the focal length of the Spectra HD cameras?

Product Line

Pelco Cameras

Environment

  • S5220 all models
  • S5230 all models
  • D5220P, D5220F
  • D5230P, D5230F

Cause

Optical millimeter range of lens for Spectra HD

Resolution

The optical millimeter (mm) range for Spectra HD

  • D5220P/F   (20X) focal length of 4.7 mm (wide) ~ 94.0 mm (tele)
  • D5230P/F   (30X) focal length of 4.3 mm (wide) ~ 129.0 mm (tele)


The following table for additional Camera/Optics information