In declaring variable, the binding qualifier PUBLIC gets error Unsupported feature when saving script program.

Issue

In declaring variable, the binding qualifier PUBLIC in a BACnet b3 controller's script program such as "Numeric Public numPoint" gets error "Unsupported feature" when saving script program.

Product Line

SmartStruxure Solution

Environment

AS

BACnet b3 controller

Script

Numeric

Public

Cause

Wants to make a Numeric variable be both the readable and writable in BACnet b3 controller script programming.

Resolution

The Public qualifier is supported in AS script program only.  

For BACnet controller script programming, use Input and Output qualifier and bind to the same object's property outside the program.

.