Is it possible to turn off the motion movement of the Esprit PTZ when it is powered up?

Issue

Can I turn off the configuration sequence of the Esprit? It is hitting a boundary pipe when powered on.

Product Line

Pelco Cameras

Environment

  • ES4036, ES4136
  • ES40P36, ES41P36-5N 
  • Esprit

Cause

The Esprit is mounted next to a pipe and it will hit the pipe when the power it is powering up.

Resolution

The Esprit series feature a mechanical self check when power is applied. The System will begin pan/tilt motion and will end self-motion within a 10 second time frame. The Esprit features no programming option to disable the Configuration Sequence at power up. 

A SMR or Special Modification Request is an option to consider for disabling of the Configuration Sequence.