Change Main Monitor Views on the DX4xxx using the Remote control.

Issue

To display video from one channel in the single view mode using the remote control.

Product Line

Pelco Video Management

Environment

  • DX4500 Series
  • DX4600 Series
  • DX4700 Series
  • DX4800 Series

Cause

  • Server Operation

Resolution

Log in to the DVR.  Press the Main button on the remote.

The Main Monitor configuration window displays.

Select a division using the arrow keys and pressing enter.

Select a Channel using the arrow keys and pressing enter.

Select OK.

OR

Without logging in if you are on single screen you can press the camera number then the enter button to call up that camera.
If in a muliview you can press the camera number then the enter button and that camera will populate in the top left pane and the other cameras will fill in sequentially in the other panes.