Heaters on, off range for the BU4, BU5, BU6 Bullet Camera series

Issue

At what temperature do the heaters turn on/off for the BU6 camera?

Product Line

Pelco Cameras

Environment

  • BU4
  • BU5
  • BU6

Cause

Heaters turn on/off range

Resolution

The BU Series Heater On/Off rang is as follows:

Model Heater On Heater Off
BU4 5°C 16°C
BU5 5°C 16°C
BU6 4°C 7°C