Can the setpoints on a SE7600 Room Controller be locked out on the keypad so no one can modify it?

Issue

Can the setpoints on a SE7600 Room Controller be locked out on the keypad so no one can modify it?

Product Line

TAC I/A Series

Environment

SE7600 or VT7600 room controllers

Cause

Design feature

Resolution

There are three keypad lockout levels:

0 = Full access to both occupied and unoccupied setpoints
1 = Temporary override capability for both occupied and unoccupied setpoints
2 = No access to both occupied and unoccupied setpoints

Review the engineering guide specifications at www.viconics.com.