Is there a way to populate an array in the declaration line as in other programming languages?

Issue

Is there a way to populate an array in the declaration line as in other programming languages i.e. Numeric numbers[4] = {1, 2, 4, 8}?

Product Line

SmartStruxure Solution

Environment

StruxureWare for Building Operation Script Editor

Cause

When defining an array in Script Editor the user may wish to populate the array with initial values.

Resolution

The way to populate an array in Script Editor is to initialise each element individually.