How do you enable or disable camera's on the DX4500/DX4600.

NOTICE

DISCONTINUED PELCO PRODUCT.
This product has been discontinued. For further information please visit pelco.com/support/discontinued-products

Issue

How do you enable or disable camera's using DX4500/DX4600 Client software. 

Product Line

Pelco Cameras, Pelco Video Management

Environment

  • DX4500
  • DX4600
  • DX4500_DX4600 Client software

Cause

System setup information

Resolution

Login using an Administrator account.

  1. Once logged into the system, click on the Setup  icon.
  2. Navigate to the Camera  menu and turn Disabled to ON or OFF.
     
  3. Exit Menu to Save changes.
     

Note: When disabling a camera the live display window will show video loss even though the input is disabled. To show a Pelco symbol you will need to loop a working camera to input you disabled.