Media Test Failure on the DVR5300.

Issue

DVR5300 does not boot all of the way up. Messages scroll across the screen saying:

  • Media test failure
  • Exiting Intel boot agent

Product Line

Pelco Video Management

Environment

DVR5300- All versions

Cause

DVR is set to boot from a LAN device.

Resolution

  1. Reboot the DVR5300 and tap the delete key to get into the BIOS.
  2. Move to the Boot tab.
  3. Select the LAN device and disable it.
  4. Save and exit the BIOS.