Document Limitations in SmartStruxure

Issue

When documents are added to SmartStruxure using the document object there are size limitations to take into consideration.

Product Line

SmartStruxure Solution

Environment

Documents

Document Object

Size Limitations

Cause

When adding a document using the document object that is larger than 20 MB the following error window pops up.

Resolution

Make sure you know the size of the file you are importing into the document object. Multiple document objects can be created again make sure the file size is below the size limit. There is not a known limit on document objects.

 

The online help file states the size limit is 17 MB. The current workaround is to use the TGML snippet execute to link directly to the file for a graphic.

In StruxureWare Building Operation 1.5 you will be able to use the hyperlink object to link directly to a file