Alarms from Pelco devices in Continuum

Issue

Video integrations with Cyberstation want to bring in Pelco based alarms

Product Line

Andover Continuum

Environment

Pelco DVR/SRV and encoders

Continuum

Windows XP

Windows 7

Windows Server 2003

Windows Server 2008

Cause

Pelco devices have alarm abilities, but not all can be brought into Continuum

Resolution

Offline and motion alarms can be brought into Continuum. Any other Pelco hardware related alarms (i.e. dry contact or alarm inputs) cannot be brought into Continuum.

See Lessons Learned article: http://buildingskb.schneider-electric.com/view.php?AID=6065  for troubleshooting motion or offline alarms