Are the EH8000RKIT refillable for dry nitrogen?

Issue

Can I get the EH800RKIT refilled when I use all of the nitrogen?

Product Line

Pelco Cameras

Environment

  • EH8000RKIT

Cause

Used entire dry nitrogen charge of EH8000RKIT

Resolution

The EH8000RKIT is a nonrefillable product. It is recommended to purchase additional kits should the amount of product installation require.