Enable Beep On Alarm Audible in DS ControlPoint.

Issue

Allows you to receive a pop-up notification when an alarm occurs on any connected system.

Product Line

Pelco Video Management

Environment

  • DS Control Point  version 7.5.609

Cause

  • Configuration

Resolution

The Login profile must be assigned Alarm Activity rights in DS Admin.

Click On Setup Alarm Popup.

Configure Alarm Pop up to Show the Alarms TAB.

From Live View click on Alarm page . The Alarm TAB opens.  Click on the beep on alarm Icon   to toggle Enable/Disable.