What are the System Requirements for Device Utility 2?

Issue

Will the device utility work with Windows 8?

Product Line

Pelco Cameras

Environment

  • Sarix Series cameras
  • DU2

Cause

Device Utility and Windows 8 compatibility

Resolution

System Requirements for Device Utility 2

Processor: Intel® Pentium® III or equivalent processor, 800 MHz

Operating System: Microsoft® Windows® XP SP4, Windows Vista® (Enterprise or Ultimate), or Windows 7 (32-bit and 64-bit); Enterprise or Ultimate, or Mac® OS x 10.8

Memory: 128 MB RAM (256 recommended)


NOTES:

  • Administrative permissions for the computer you are using to install Device Utility 2 is required.