Rooftop mount option for Esprit series

Issue

How to mount Esprit for rooftop application.

Product Line

Pelco Cameras

Environment

  • ES4036 Series
  • ES4136 Series
  • ES40P36 Series
  • ES41P36 Series
  • ES3012

Cause

Application to meet the installation design of mounting Esprit on the top off a flat roof.

Resolution

The Esprit series support rooftop mount options with the following parts:

Note: Image below is referenced for Esprit ImagePak that includes wall mount. (EWM)

  1. Esprit image pak with EWM, or Esprit with separate order of EWM.
  2. EA4348 (plate image)
  3. PP4348 (rooftop mount)