Values on graphic pages constantly showing 'down' momentarily

Issue

Values on graphic pages constantly showing 'down' momentarily
The following message can be seen in the standard output.

"duplicate server session kills"

Product Line

TAC I/A Series

Environment

I/A Series R2 Enterprise Server

Cause

There is another copy of the same Enterprise Server station running on the network. In this particular case, there is a another computer on the network that has been licensed as an Enterprise Server and it has a copy of the Enterprise Server station. This computer is meant as a standby computer and the Enterprise Server station should not be running. 

Resolution

In this particular case, there is a another computer on the network that has been licensed as an Enterprise Server and it has a copy of the Enterprise Server station. This computer is meant as a standby computer and the Enterprise Server station should not be running. 

Stop the Enterprise Server station that is running on the standby computer. From the Admin Tool, connect to the localhost and right click on the Enterprise Server station. Make sure auto run is uncheck.