DX2000 Minimum PC Requirements for Remote Site Software

NOTICE

DISCONTINUED PELCO PRODUCT.
This product has been discontinued. For further information please visit pelco.com/support/discontinued-products

Issue

DX2000 Remote Site PC Requirements

Product Line

Pelco Video Management

Environment

  • DX2008
  • DX2016
  • Remote PC

Cause

PC system requirements for connection to DX2000

Resolution

Minimum PC Requirements for Remote Site Software of the DX2000:

  • Pentium III processor; 800 Mhz; 128 MB RAM;
  • 1024 x 768 display resolution; 24-bit color display;
  • Video card with 16 or more megabytes of RAM;
  • Windows 2000, NT 4.0 (SP6), XP, ME;
  • Internet Explorer 5.5 through Internet Explorer 6 only.
  • Ethernet-compatible network card (10/100 preferred)
     
  1. Note: Installation of msjava86 from the Pelco ftp site will be required: https://schneider-electric.box.com/s/ah8wjzv0ke3sngg8xr39nuiavpvh7mhw
  2. Non installation of msjava86 will result in page continuously attempting to load.
  3. Loading of msjava will prompt the additional load requirements of Netframe and Active X.

 
Note: Product has been discontinued. Information provided to assist with active field product.