DVR5100 Series Recorder- How to activate patterns, presets, and scans.

Issue

How to program patterns, presets to a ptz camera from DVR5100 Recorder.

Product Line

Pelco Video Management

Environment

DVR5100 Hybrid Video Recorder

Cause

Program patterns, presets, and scans to analog Spectra ptz cameras.

Resolution

PATTERNS

ACTIVATING PATTERNS

To activate a pattern from the DVR5100, complete the following steps:

1. From the main menu, select Actions. The Actions menu appears.

2. Navigate to PTZ Operations, and then press Enter/Shift. The PTZ Operations dialog box appears.

3. On the Panel Keypad press + or - key until the pattern number appears in the text field.

4. Press the blue function key. The pattern starts. To exit the dialog box without activating the pattern, press the

red function key.

STOPPING A PATTERN

To stop a pattern using the DVR5100, complete the following steps:

1. Select the video pane that is displaying video from a camera running a PTZ pattern.

2. If the border of the selected video pane is green, Press Enter/Shift. The border color changes to blue.

3. Move the joystick any direction. The pattern stops.

PRESETS

ACTIVATING PRESETS

To activate a preset from the DVR5100, complete the following steps:

1. While in live view mode, select a video pane that is displaying video from a camera with PTZ capabilities. The

video pane border is green.

2. From the main menu, select Actions, and then press Enter/Shift. The Action menu appears.

3. Select PTZ Operations, and then press Enter/Shift, The PTZ Operations dialog box appears.

4. On the Panel Keypad press + or - key until the preset number appears in the text field, and then press the

yellow function key. The camera is moved to the preset location. To cancel your selection without activating

the preset, press the red function key.

SCANS

ACTIVATING SCANS

To scan is to view an area by panning a camera horizontally to the right or left. There are three types of

scans available:

Scan Random: A random scan occurs when the camera pans in an irregular, unsystematic pattern.

Scan Frame: A frame scan occurs when the camera is repositioned for a three-second interval scan

followed by a three-second pause.

Scan Auto: An auto scan occurs by panning a camera continuously to the left or right.

To activate scanning using the DVR5100, complete the following steps:

1. While in live view mode, select a video pane that is displaying video from a camera with PTZ capabilities.

The video pane border is green.

2. From the main menu, select Actions, and then press Enter/Shift. The Action menu appears.

3. Select PTZ Operations, and then press Enter/Shift, The PTZ Operations dialog box appears.

4. On the Panel Keypad press + or - key until the scan number appears in the text field, and then press

the yellow function key. The camera scans according to the actions. To cancel your selection without

activating the scan, press the red function key.