Connect the FTV/FRV Series Fiber modules to the DX4104 series DVR For Video and PTZ (Pan, Tilt, and Zoom) control.

Issue

How do I integrate the FTV series modules; wiring and setup for PTZ control.

Product Line

Pelco Video Management

Environment

  • DX4104 Series DVR.
  • FTV10D1 FRV10D1 Fiber Modules
  • FTV40D  FRV40D Fiber Modules
  • FTV80D  FRV80D Fiber Modules

Cause

  • Installation and Service
  • There are no Data LEDs blinking on the Fiber Modules.
  • There is not any PTZ control.

Resolution

To configure the DX4104 Series DVR for PTZ control read: How to Set Up PTZ Control over 2 wires on the DX4100 DVR

The Video must be connected to the fiber modules for PTZ control. Wire per diagram:

Refer to the PTZ camera Installation Operation Manual for Switch settings to correspond with the DVR outputs; Pelco P or Pelco D protocol.

 

Note* When controlled the DATA IN LED blinks on the fiber receiver, and the DATA OUT LED blinks on the fiber transmitter.