What are the power requirements for an Esprit IP ptz camera?

Issue

Power requirements

Product Line

Pelco Cameras

Environment

Esprit IP: All versions

Cause

Current draw

New installation

Camera reboots when its cold outside

No ptz

Resolution

Input Voltage 24, 120, or 230 VAC, 50/60 Hz. The ESTXE-2 is for the Esprit IP models that require 24V input and the ESTXE-5 is for the Esprit IP models that require a 120/240 V input.

Switch selectable for 120/230 VAC inputs.

Input Voltage Range ±10%.

Power Consumption Maximum 75 VA per system.

 Esprit IP Specification Sheet