NOTICE
POTENTIAL FOR DATA LOSS.The steps detailed in the resolution of this article may result in a loss of critical data if not performed properly. Before beginning these steps, make sure all important data is backed up in the event of data loss. If you are unsure, please contact Product Support Services prior to attempting the procedure below.
NOTICE
COMPLEX PROCEDURE REQUIRED.The resolution of this article has many complex steps that may result in unforeseen results if not performed correctly. If you are at all unfamiliar with the requirements, please contact Product Support Services for assistance.
Issue
You wish to prevent your cameras from being discovered automatically on the network.
Product Line
Pelco Cameras, Pelco Video Management
Environment
Pelco Sarix cameras, all versions
Cause
Sarix cameras support Universal Plug and Play (UPnP) out of the box. This allows them to be discovered automatically in Endura systems.
Resolution
Sarix 1.0 cameras
- Download and install the latest version of Endura Utilities. Click here for instructions on how to do so.
- Open Endura Utilities and press Search.
- Right-click on the camera you wish to modify and choose Device Actions → Enable SSH
- Right-click on the camera again and choose Scripts → One-time script
-
For the content, enter in the following:
mv /etc/init.d/ev-compat /etc/init.d/ev-compat.old
reboot
Sarix 2.0 (Enhanced) cameras
- Download and install the latest version of Endura Utilities. Click here for instructions on how to do so.
- Open Endura Utilities and press Search.
- Right-click on the camera you wish to modify and choose Device Actions → Enable SSH
- Right-click on the camera again and choose Scripts → One-time script
-
For the content, enter in the following:
mv /etc/systemd/system/ev-compat.service /etc/systemd/system/ev-compat.service.old
/sbin/restart.sh
Sarix 3.0 (Professional) cameras
It is not possible to disable UPnP on a Sarix Professional camera.
Note: These actions will prevent your camera from being discovered in Endura Utilities and will break any functionality with an Endura system. However, Digital Sentry does not use UPnP and will continue to function normally.