Can I use PoE to power the Spectra HD environmental dome camera?

Issue

Can I use PoE to power the Spectra HD environmental dome camera?

Product Line

Pelco Cameras

Environment

  • S5220-YB0 S5230-YB0 S5220-YB1
  • S5230-YB1 S5220-EG0 S5230-EG0
  • S5220-EG1 S5230-EG1 S5220-ESG0
  • S5230-ESG0 S5220-ESG1 S5230-ESG1

Cause

Power for the S5220-EG1..

Resolution

PoE will not work for power to the environmental Spectra HD dome they require more power than PoE can supply. It is recommended to use the WCS1-4 or WCS4-20 to power the environmental Spectra HD dome.

Note: Spectra HD support both NTSC and PAL power. It required 24 VAC, 23 VA nominal (without heater and blower); 73 VA nominal (with heater and blower) 24 VDC, 0.7 A nominal (without heater and blower); 3 A nominal (with heater and blower)

Recommand power supply: MCS Series or WCS Series