What actuators can be used with the VG210R and VG310R ball valves ranges?

Issue

What actuators are available?

Product Line

Field Devices

Environment

VG210R

VG310R

Actuators

Cause

Choice of available actuators.

Resolution

Suitable Actuators for the VG210R and VG310R ball valves ranges are;

Direct fit.

  • MG600C,
  • MG600C SR

 

With AV-823 Long Stem adaptor.

  • M400
  • M800
  • M1500
  • MG900 SR

To view the following data sheets, please select the data sheet required.

VG210RVG310R, MG600CMG600C InstallationMG600C SRMG600C SR Installation and Manual Override instructions