What lens can I use with the C20-CH-6 or C20-DW-6?

Issue

What lens can I use with the C20-CH-6 or C20-DW-6?

Product Line

Pelco Cameras

Environment

  • 13VD1-3 13VD2.5-6 13VD2.8-12 13VD3-8
  • 13VD5-40 13VD5-50 13VD5.5-82.5 13VD15-50
  • C20-CH-6
  • C20-DW-6

Cause

Replacing old Pelco box camera and need a lens to work with the new C20-CH-6 or C20-DW-6.

Resolution

Recommended lenses for the C20 Series cameras:

  • 13VA/13VD Series: Varifocal lenses, 1/3-inch format; 13VA (manual iris); 13VD (auto iris, DD)
  • 13ZD: Motorized zoom lenses, 1/3- inch format (auto iris, DD)
  • 13VDIR Lenses