What is part number for the power transformer to the FR82011MSTR-1?

Issue

I need the part number for the power transformer for the FR82011MSTR-1?

Product Line

Pelco Transmission & Power

Environment

  • FT82011MSTR-1 FR82011MSTR-1
  • FT82011MSCR-1 FR82011MSCR-1
  • FT82011SSTR-1 FR82011SSTR-1
  • FT82011SSCR-1 FR82011SSCR-1
  • FT85011AMSTR / FR85011AMSTR

Cause

Transformer part replacement required

Resolution

The part number to order a replacement transformer is PS04-1502-0512 for the FR82011MSTR-1. 2 Position Power Terminal block pn# CN02-2606-3102G