Can I get a fiber transmitter install into the ExSite IP Series Explosion proof Network Camera System?

Issue

Can I get a fiber transmitter install into the ExSite IP Series Explosion proof Network Camera System?

Product Line

Pelco Cameras, Pelco Transmission & Power

Environment

  • IPSXME036-2, IPSXME036-2X, IPSXME036-7, IPSXME036-7X, IPSXME136-2, IPSXME136-2X, IPSXME136-7, IPSXME136-7X
  • EHXME036-2, EHXME036-2X, EHXME036-7, EHXME036-7X, EHXME123-2, EHXME123-2X, EHXME136-7, EHXME136-7X

Cause

Customer is needing both fiber and Network connections at the same time.

Resolution

Due to the fact that the ExSite camera systems have only one plug-in connector for use with the TXB series boards, there cannot be two TXB board installed at the same time in the same product. This also includes the Esprit and Spectra series cameras.

The TXB board in question is either the TXB-N for TCP/IP connections, or Protocol TXB converters (TXB-V, TXB-B, etc.), OR the FS85011 fiber modules.