What matrix system replaces the CM9500?

NOTICE

DISCONTINUED PELCO PRODUCT.
This product has been discontinued. For further information please visit pelco.com/support/discontinued-products

Issue

I have the old CM9500 system what matrix would I use to replace this system?

Product Line

Pelco Matrix

Environment

  • CM9502 CM9501
  • CM6700-MXB4
  • CM6800-32X6 CM6800E-48X8
  • CM6800-96X16

Cause

Replacement for CM9500 matrix system. 

Resolution

  • CM6700-MXB4 - The CM6700 Series features 16 camera inputs with looping outputs. The maximum monitor outputs are 4. Keyboards supported are the KBD100, KBD200A, KBD300A.
  • CM6800-32X6 -  The CM6800-32X6 is  32 camera inputs with 6 monitor outputs. Keyboards supported are KBD100, KBD200A, KBD300A, KBD960
  • CM6800E-48X8 - The CM6800E-48x8 is a 48 camera input with 8 monitor outputs. Keyboards supported are KBD100, KBD200A, KBD300A, KBD960
  • CM6800-96X16 - The CM6800-96X16 is a 96 camera input with 16 monitor outputs. Keyboards supported are KBD100, KBD200A, KBD300A, KBD960