How many KBD4000 or KBD4002 can I connect to a Genex multiplexor

Issue

How many KBD4000 or KBD4002 can I connect to the Genex multiplexor?

Product Line

Pelco Video Management

Environment

  • KBD4000
  • KBD4002

Cause

Adding more then one KBD4000 or KBD4002  to a Multiplexor.

Resolution

You can only connect 1 KBD4000 or KBD4002 to the Multiplexor. To connect more than 1 KBD4000 or KBD4002 you must use the MX4000SVR.The you can have a maximum of 4 KBD4000 or KBD4002 connected to the MX4000SVR.