Can I use the DF5-BKT in the Spectra IV outdoor housing?

Issue

Can I use the DF5-BKT in the Spectra IV outdoor housing?

Product Line

Pelco Cameras

Environment

  • DF5-BKT
  • DF5 Series
  • Spectra IV Series

Cause

A request to install a fixed camera in the Spectra IV Environmental Housing.

Resolution

The DF5-BKT is only designed to function within the DF5 Series fixed dome housing. It is not compatible with the Spectra IV housings.