Xenta Server can't receive some values from M-bus meter

Issue

Can't receive "Power Factor" values from ABB's M-bus meters.

Product Line

TAC Vista

Environment

Xenta 913
Xenta 701
Xenta 711
Xenta 721
Xenta 731

Cause

Earlier versions of X700/ X913 system software did not support M-bus manufacturer specific data that contains extra status information in the VIFE

Resolution

For Xenta 700, there is a hotfix for v5.1.8 that adds support for this type (also included in v5.1.9 and later) .

For Xenta 913, v5.1.9 and later includes this hotfix.