Is there a way to determine which version of Operator Interface is installed without actually running the program?

Issue

Is there a way to determine which version of Operator Interface is installed without actually running the program?

Product Line

TAC I/A Series

Environment

DMS

Operator Interface

Cause

Determine the version without running the program

Resolution

Open the file LANGUAGE.TXT in the DMS folder using Notepad and line 12 will indicate the version installed: