What is the part number for the battery in the CM6700-MXB2 or CM6700-MXB4?

Issue

What is the part number for the battery in the CM6700-MXB2 or CM6700-MXB4?

Product Line

Pelco Cameras

Environment

  • CM6700-MXB2, CM6700-MXB2-X
  • CM6700-MXB4, CM6700-MXB4-X

Cause

All programming is lost (erases) after a power outage occurs. 

Resolution

The CM6700 matrix features a replaceable lithium coin battery that provides data protection. It is required to remove the cover of the CM6700 in order to access the clip held battery.The Pelco part number for the battery is BATLCCBR2330. Nominal Voltage is 3 V.