TAC Xenta 471 cannot accept a thermistor input

Issue

Can I connect a thermistor to a TAC Xenta 471?

Product Line

TAC Vista

Environment

  • Xenta 471 I/O module
  • Thermistor sensor

Cause

Xenta 471 does not have any thermistor inputs.

Resolution

TAC Xenta 471 has 8 analog inputs that can be set up as current inputs (0/4-20mA with external power and 4-20 with internal power) or as voltage inputs (0-1, 0/2-10 V DC).