How to create a temporary macro using a CM9700 Matrix Keyboard (CM9760-KBD)

Issue

A quick camera sequence is desired.

Product Line

Pelco Monitors

Environment

CM9760-KBD all versions

Cause

Pelco System Manager is not available.

Resolution

When using the define key (DEF) the default PIN number is 1-2-3-4