Unable to select and save Sarix IM10LW10 analytic behaviors.

Issue

Unable to check mark the Analytics of Adaptive Motion or Camera Sabotage from Sarix web page.

Product Line

Pelco Cameras

Environment

  • IM10LW (version 1.8 through 1.9.12)
  • IE Internet Explorer

Cause

Programming behavior of adaptive motion.

Resolution

SARIX ANALYTICS

The selected behavior (highlighted in web page) is normally enabled once the "activate behavior" feature is check marked. If the selected behavior does not enable then it is recommended to enable compatibility view of the web page. Ensure to add the website (cameras IP address) to IE compatibility view settings page.