Veris temperature transmitter - control system is reading an inaccurate temperature reading

Issue

Veris temperature transmitter - control system is reading an inaccurate temperature reading

Product Line

Field Devices

Environment

Veris temperature sensor with voltage transmitter output

Cause

The Veris sensor and the controller are located at different locations and using a different common as they are being powered by different power sources. 

Resolution

Refer to the sensor's installation instructions and ensure that the sensor and controller uses the same common.