What is power supply part number for KBD960?

Issue

  • The CM9505UPS is obsolete, what is the replacement?
  • What replaced the KBD960 power supply?

Product Line

Pelco Matrix

Environment

KBD960

  • CM9505UPS
  • KBD960-US
  • PS01-3002-9015G

Cause

The CM9505UPS has no listed replacement available for reference.

Resolution

The KBD960 is the older part number and this keyboard came with the CM9505UPS. Due to the new keyboards,  KBD960-US, having a new power supply, the valid replacement to the CM9505UPS will be the PS01-3002-9015G. Also select proper power cord part number from list for region. A suffix of -US, -UK, -AU, or -EU, designating a region-specific power cord, is added to the above model numbers when ordering. For example, a KBD960-US is a desktop keyboard with a power cord for use in the United States. Select the proper power cord:

  • US-320-C5
  • UK-320-C5
  • AU-320-C5
  • EU-320-C5