Sarix Professional IMP Series Back Box Part Numbers.

Issue

BOM does not provide a part number for the Back Box on Indoor and Environmental Back Boxes.

Product Line

Pelco Cameras

Environment

  • IMP519 Series
  • IMP319 Series
  • IMP219 Series
  • IMP110 Series
  • IMPS110 Series
  • IMPBB-I
  • IMPBB-S
  • IMPBB-P
  • IMPBB-Ei
  • IMPBB-ES
  • IMPBB-EP

Cause

Order Process, Installation, and Service.

Resolution

 

NOTE* If the IMPBB-P is purchased, the customer must use the WMVE-SW for a Mount, because the .75 inch to 1.5 inch NPT adapter comes with the mount.

________________________________________________________________________________________

 

Related Topics:

How do I Connect the Sarix Professional IMP series Indoor Pendant to the WMVE-SW mount.