Controller locks up on configuration of the Modbus TCP-IP XDriver.

Issue

Controller locks up on configuration of the Modbus TCP-IP XDriver.

Product Line

Andover Continuum

Environment

Continuum Controller

Cause

The Device Comm Status point was created as an InfinityString instead of InfinityNumeric

Resolution

Delete the incorrect Device Comm Status point and re-create it appropriately as an InfinityNumeric.