Enable / Disable Email Delivery From a Graphic

Issue

Have the ability in SBO to disable and enable the email delivery from a graphic with a simple switch

Product Line

SmartStruxure Solution

Environment

Automation Server (AS), Enterprise Server (ES) - all versions

Cause

- none -

Resolution

In order to enable / disable email delivery from a graphic, do the following:

1. Add a Switch component to a graphic. Save the graphic.
2. In Workstation, open the bindings window for the graphic. Bind the Status of the Email Notification to the Value of the Switch.