What is the part number for the pedestal mount to go with the ExSite IP Series Fixed Explosion Proof Camera System?

Issue

What is the part number for the pedestal mount to go with the ExSite IP Series Fixed Explosion Proof Camera System?

Product Line

Pelco Cameras

Environment

EHXME036-2, EHXME036-2X, EHXME036-7, EHXME036-7X, EHXME123-2, EHXME123-2X, EHXME136-7, EHXME136-7X

Cause

Customer wanted the part number for the pedestal mount to work with ExSite IP Series Fixed Explosion Proof Camera System.

Resolution

Use the PXM100 pedestal mount for use with the ExSite IP Series, Fixed, or PTZ explosion proof camera systems.

 

More information about these mounts can be found here: C1300.