Will the BU4-IRF4-4 work with a non Pelco DVR?

Issue

Will the BU4-IRF4-4 work with a non Pelco DVR?

Product Line

Pelco Cameras

Environment

BU4-IRF4-4, BU4-IRF4-4X

Cause

Customer is replacing non Pelco camera with the BU4-IRF4-4.

Resolution

Yes as long as the non-Pelco DVR accepts the NTSC or Pal format analog/composite video, the use of the BU4-IRF4-4 analog camera will work.