Can I get an analog output on the Esprit IP Positioning System?

Issue

Can I get an analog output on the Esprit IP Positioning System?

Product Line

Pelco Cameras

Environment

Esprit IP- All versions

Cause

Customer would like to use analog and IP from the same ES41E36-5N Esprit IP based model.

Resolution

The Esprit IP based camera systems, due to the design, do NOT have the capability of providing both analog/composite video (out of a BNC) and video via Ethernet at the same time. However, as a related side note, a Spectra IV IP dome system CAN provide BOTH the analog/composite video and TCP/IP Ethernet video.