Issue
Can the FD5 Series camera be mounted on a wall with conduit coming in from a specific direction?
Product Line
Pelco Cameras
Environment
- FD5 Series Camera
Cause
Requirement to mount the FD5 Series camera with conduit coming in from a specific direction. Video displayed needs to be correct orientation.
Resolution
The camera within the FD5 Series does have the ability to rotate along multiple axis. The camera can be mounted with conduit coming into the side conduit thread hole 7/8" diameter from the direction that is required, then the camera rotated to match the correct orientation.